OPC UA - Troubleshooting

If the connection to the server cannot be established, verify if the:

  • Correct server IP and port are configured within the client configuration.
  • Runtime Service can open the configured OPC UA listening port successfully.
  • Machine running the Runtime Service can be reached within the network (e.g., ping command).
  • Passwords for the server and client configuration match.
  • Correct certificates are used.
  • Correct security policy is configured for server and client.