Read and Write PLC Variables via HTTP Interface
The PLC variable interface provides these features and advantages:
- A simple HTTP interface is used to read/write PLC variables.
- Multiple variables can be read /written in single HTTP request at the end or start of a PLC cycle.
- Quick application development.
- The interface allows a user to quickly develop applications in many languages (e.g., Java, C#, and C++).
- Platform independence.
- Applications can be developed on any platform supporting HTTP.
- Remote access.
- Variables may be read/written from a remote machine.
- Security.
- There is an Authorization mechanism which enables access to the interface.
- See Configure the Controller.
- Support for both JSON and text (raw) formats to send/receive requests or responses.
- Support for all basic PLC data types:
BOOL
SINT
USINT
BYTE
INT
UINT
WORD
DINT
UDINT
DWORD
LINT
ULINT
LWORD
REAL
LREAL
TIME
STRING
There are two interfaces:
- A variable READ interface which is used to read a set of PLC variables.
- A variable WRITE interface which is used to write a set of PLC variables.
The URL is same for both interfaces: (controller URL)/kas/plcvariables