EtherCAT Topology

Using full-duplex Ethernet physical layers, EtherCAT slave controllers close an open port automatically and return the Ethernet frame if no downstream device is detected.

  • Slave devices can have several ports.
  • Using these features, EtherCAT can support almost any physical topology (e.g., line, tree, or star).
    • The bus or line structure known from the fieldbuses is then available for Ethernet.

The combination of line and branches or stubs is also possible.

  • Any EtherCAT device with three or more ports can act as a junction; no additional switches are required.
  • The classic switch-based Ethernet star topology can be used either with switches configured to forward traffic directly between ports, or with special slave devices.
    • The switches are then located between the network master and the slave devices.

The special slave device assembly (i.e., standard slave devices don't have a MAC address) attached to one switch port together forms an EtherCATsegment. This is either addressed via its MAC address or via port-based VLANs.

  • Since the 100BASE-TX Ethernet physical layer is used, the distance between any two nodes can be up to a maximum of 100 m (300 ft).
  • Up to 65535 devices can be connected per segment.
  • If an EtherCAT network is wired in ring configuration (requiring two ports on the master device), it can provide cable redundancy.

Flexible Topology: Line, Tree or Star

Figure 1: Flexible Topology: Line, Tree, or Star

  • KAS controllers support line, tree, and star topologies.
  • Ring topologies and cable redundancy is not supported because the KAS controllers have a singe EtherCAT port.

Concept Link IconSee Also