Add the Controller

  1. In the File menu, click New to start the Controller Creation Wizard.
  2. Select the type of controller in the project.

    Figure 1: Choose controller type dialog

  3. Choose the motion engine option (Pipe Network Concept or PLCopen) and select the application template.

    Figure 2: Choose an application template dialog

  4. Click Finish.
  5. In the File menu, click Save As.
  6. Define the Project Name and its location.
  7. Click OK.