Start the KAS-IDE

There are multiple ways to start the KAS-IDE.

  • Double-click a desktop shortcut.
  • Double-click a project file to open it with the most recently installed version of the KAS-IDE.
  • Windows 10 and 11: From the Start menu, under "K".

    • The KAS-IDE supports simultaneously running multiple instances.
    • Double-click a shortcut or project file, or selecting the application from the Start menu, opens another instance.
    • Double-click a project file more than once opens a copy of the project in another instance of the KAS-IDE.

See the these FAQs for more options: