Home tab
To access the KAS Kollmorgen Automation Suite web server home The homing procedure allows, based on a position measurement, to set a position offset to the motor to ensure it is physically at the home position. page, enter the controller's IP address.
This page provides an overview of the device including:
- Manufacturer
- CPU Speed Speed is the absolute value of the velocity without direction.
- CPU Cores
- Model Number
- See Controllers for more information.
- Serial Number
- Hardware Revision
- TCP Tool Center Point - The point in the machine that is commanded to move, typically the center or the head of the tool. It can be described in different coordinate systems./IP MAC Address A Media Access Control (MAC) address is a quasi-unique identifier assigned to most network adapters or network interface cards (NICs) by the manufacturer for identification. If assigned by the manufacturer, a MAC address usually encodes the manufacturer's registered identification number. — a unique value associated with the TCP/IP network adapter that uniquely identifies the adapter on a LAN.
- EtherCAT Ethernet ofr Control Automation Technology. EtherCAT® is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT is to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs. MAC Address — a unique value associated with the EtherCAT network adapter that uniquely identifies the adapter on an EtherCAT network.
-
-
Unless otherwise noted, any reference to AKD PDMM or PCMM refers to both the 800MHz and the single- and dual-core 1.2GHz variants.