Create Control Panel Views

Control Panels are created and managed in the KAS-IDE Project Explorer.

  1. In the Project Explorer tree, right-click the Controller and select Add Control Panel. (Figure 1)
  2. Figure 1: Add Control Panel option

  3. Right-click the new Panel and select Rename. (Figure 2)
  4. Figure 2: Rename option

    The Renamedialog box opens.

  5. Change the Panel name. (Figure 3)
  6. Figure 3: Rename dialog box with changed name

  7. Click OK to save the changes or selections and close the dialog box.
  8. In the Project Explorer tree, double-click the new Control Panel to open it in the KAS-IDE graphical editor. (Figure 4)
  9. Figure 4: New Control Panel