Enums tab
This tab allows you to define enums (Enumerated Types). An enumerated type allows you to define a data type and assign a specific set of accepted values. 
Adding Enums
An enum may be created in one of these ways:
- Right-click within the Enum tab and select Insert Enum.
- Press the Insert key while the Enum tab is active.
This creates a default enum labelled as "EnumTypen" with the Value of "V0,V1".
Double click on the Type or Value to make changes.
-
-
- An enum must contain two or more values.
- If only one value is defined, it is not considered and the previous value is retained.
- An enum cannot contain special characters (e.g., #, @, etc.)
- If a special character is defined in the value field, it is not considered and the previous value is retained.
Create Enums
- Enter the enum type and hash (#), the press Ctrl+Space.
This opens a dialog to select the corresponding value.
- Select the value and click the check mark.
The value is loaded into the program.
Declaring Enums
Enums may be declared in the same way as variables; at the end of the line press Enter.
As CurrentDrive is not a part of the dictionary, a dialog is opened to add the variable. Set the Types as the enum name. 
Once this is added, the variable will be displayed with the selected type in the Dictionary.