ACTION#.ACTIVE

Description

Sets whether an action is disabled or enabled. When set to 1, the action will be executed if it is valid.

Value Description
0 Action disabled
1 Action enabled

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

ACTION1.ACTIVE

3900h

01h

Unsigned8

-

-

Read/Write

No

ACTION2.ACTIVE

3900h

02h

Unsigned8

-

-

Read/Write

No

ACTION3.ACTIVE

3900h

03h

Unsigned8

-

-

Read/Write

No

ACTION4.ACTIVE

3900h

04h

Unsigned8

-

-

Read/Write

No

ACTION5.ACTIVE

3900h

05h

Unsigned8

-

-

Read/Write

No

ACTION6.ACTIVE

3900h

06h

Unsigned8

-

-

Read/Write

No

ACTION7.ACTIVE

3900h

07h

Unsigned8

-

-

Read/Write

No

ACTION8.ACTIVE

3900h

08h

Unsigned8

-

-

Read/Write

No

ACTION9.ACTIVE

3900h

09h

Unsigned8

-

-

Read/Write

No

ACTION10.ACTIVE

3900h

0ah

Unsigned8

-

-

Read/Write

No

ACTION11.ACTIVE

3900h

0bh

Unsigned8

-

-

Read/Write

No

ACTION12.ACTIVE

3900h

0ch

Unsigned8

-

-

Read/Write

No

ACTION13.ACTIVE

3900h

0dh

Unsigned8

-

-

Read/Write

No

ACTION14.ACTIVE

3900h

0eh

Unsigned8

-

-

Read/Write

No

ACTION15.ACTIVE

3900h

0fh

Unsigned8

-

-

Read/Write

No

ACTION16.ACTIVE

3900h

10h

Unsigned8

-

-

Read/Write

No

ACTION17.ACTIVE

3900h

11h

Unsigned8

-

-

Read/Write

No

ACTION18.ACTIVE

3900h

12h

Unsigned8

-

-

Read/Write

No

ACTION19.ACTIVE

3900h

13h

Unsigned8

-

-

Read/Write

No

ACTION20.ACTIVE

3900h

14h

Unsigned8

-

-

Read/Write

No

ACTION21.ACTIVE

3900h

15h

Unsigned8

-

-

Read/Write

No

ACTION22.ACTIVE

3900h

16h

Unsigned8

-

-

Read/Write

No

ACTION23.ACTIVE

3900h

17h

Unsigned8

-

-

Read/Write

No

ACTION24.ACTIVE

3900h

18h

Unsigned8

-

-

Read/Write

No

ACTION25.ACTIVE

3900h

19h

Unsigned8

-

-

Read/Write

No

ACTION26.ACTIVE

3900h

1ah

Unsigned8

-

-

Read/Write

No

ACTION27.ACTIVE

3900h

1bh

Unsigned8

-

-

Read/Write

No

ACTION28.ACTIVE

3900h

1ch

Unsigned8

-

-

Read/Write

No

ACTION29.ACTIVE

3900h

1dh

Unsigned8

-

-

Read/Write

No

ACTION30.ACTIVE

3900h

1eh

Unsigned8

-

-

Read/Write

No

ACTION31.ACTIVE

3900h

1fh

Unsigned8

-

-

Read/Write

No

ACTION32.ACTIVE

3900h

20h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

40100

1

40100 (0x9ca4)

ACTION1.ACTIVE

Unsigned8

Read/Write

Yes

40101

1

40101 (0x9ca5)

ACTION2.ACTIVE

Unsigned8

Read/Write

Yes

40102

1

40102 (0x9ca6)

ACTION3.ACTIVE

Unsigned8

Read/Write

Yes

40103

1

40103 (0x9ca7)

ACTION4.ACTIVE

Unsigned8

Read/Write

Yes

40104

1

40104 (0x9ca8)

ACTION5.ACTIVE

Unsigned8

Read/Write

Yes

40105

1

40105 (0x9ca9)

ACTION6.ACTIVE

Unsigned8

Read/Write

Yes

40106

1

40106 (0x9caa)

ACTION7.ACTIVE

Unsigned8

Read/Write

Yes

40107

1

40107 (0x9cab)

ACTION8.ACTIVE

Unsigned8

Read/Write

Yes

40108

1

40108 (0x9cac)

ACTION9.ACTIVE

Unsigned8

Read/Write

Yes

40109

1

40109 (0x9cad)

ACTION10.ACTIVE

Unsigned8

Read/Write

Yes

40110

1

40110 (0x9cae)

ACTION11.ACTIVE

Unsigned8

Read/Write

Yes

40111

1

40111 (0x9caf)

ACTION12.ACTIVE

Unsigned8

Read/Write

Yes

40112

1

40112 (0x9cb0)

ACTION13.ACTIVE

Unsigned8

Read/Write

Yes

40113

1

40113 (0x9cb1)

ACTION14.ACTIVE

Unsigned8

Read/Write

Yes

40114

1

40114 (0x9cb2)

ACTION15.ACTIVE

Unsigned8

Read/Write

Yes

40115

1

40115 (0x9cb3)

ACTION16.ACTIVE

Unsigned8

Read/Write

Yes

40116

1

40116 (0x9cb4)

ACTION17.ACTIVE

Unsigned8

Read/Write

Yes

40117

1

40117 (0x9cb5)

ACTION18.ACTIVE

Unsigned8

Read/Write

Yes

40118

1

40118 (0x9cb6)

ACTION19.ACTIVE

Unsigned8

Read/Write

Yes

40119

1

40119 (0x9cb7)

ACTION20.ACTIVE

Unsigned8

Read/Write

Yes

40120

1

40120 (0x9cb8)

ACTION21.ACTIVE

Unsigned8

Read/Write

Yes

40121

1

40121 (0x9cb9)

ACTION22.ACTIVE

Unsigned8

Read/Write

Yes

40122

1

40122 (0x9cba)

ACTION23.ACTIVE

Unsigned8

Read/Write

Yes

40123

1

40123 (0x9cbb)

ACTION24.ACTIVE

Unsigned8

Read/Write

Yes

40124

1

40124 (0x9cbc)

ACTION25.ACTIVE

Unsigned8

Read/Write

Yes

40125

1

40125 (0x9cbd)

ACTION26.ACTIVE

Unsigned8

Read/Write

Yes

40126

1

40126 (0x9cbe)

ACTION27.ACTIVE

Unsigned8

Read/Write

Yes

40127

1

40127 (0x9cbf)

ACTION28.ACTIVE

Unsigned8

Read/Write

Yes

40128

1

40128 (0x9cc0)

ACTION29.ACTIVE

Unsigned8

Read/Write

Yes

40129

1

40129 (0x9cc1)

ACTION30.ACTIVE

Unsigned8

Read/Write

Yes

40130

1

40130 (0x9cc2)

ACTION31.ACTIVE

Unsigned8

Read/Write

Yes

40131

1

40131 (0x9cc3)

ACTION32.ACTIVE

Unsigned8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

ACTION1.ACTIVE

40100

Unsigned8

Read/Write

-

ACTION2.ACTIVE

40101

Unsigned8

Read/Write

-

ACTION3.ACTIVE

40102

Unsigned8

Read/Write

-

ACTION4.ACTIVE

40103

Unsigned8

Read/Write

-

ACTION5.ACTIVE

40104

Unsigned8

Read/Write

-

ACTION6.ACTIVE

40105

Unsigned8

Read/Write

-

ACTION7.ACTIVE

40106

Unsigned8

Read/Write

-

ACTION8.ACTIVE

40107

Unsigned8

Read/Write

-

ACTION9.ACTIVE

40108

Unsigned8

Read/Write

-

ACTION10.ACTIVE

40109

Unsigned8

Read/Write

-

ACTION11.ACTIVE

40110

Unsigned8

Read/Write

-

ACTION12.ACTIVE

40111

Unsigned8

Read/Write

-

ACTION13.ACTIVE

40112

Unsigned8

Read/Write

-

ACTION14.ACTIVE

40113

Unsigned8

Read/Write

-

ACTION15.ACTIVE

40114

Unsigned8

Read/Write

-

ACTION16.ACTIVE

40115

Unsigned8

Read/Write

-

ACTION17.ACTIVE

40116

Unsigned8

Read/Write

-

ACTION18.ACTIVE

40117

Unsigned8

Read/Write

-

ACTION19.ACTIVE

40118

Unsigned8

Read/Write

-

ACTION20.ACTIVE

40119

Unsigned8

Read/Write

-

ACTION21.ACTIVE

40120

Unsigned8

Read/Write

-

ACTION22.ACTIVE

40121

Unsigned8

Read/Write

-

ACTION23.ACTIVE

40122

Unsigned8

Read/Write

-

ACTION24.ACTIVE

40123

Unsigned8

Read/Write

-

ACTION25.ACTIVE

40124

Unsigned8

Read/Write

-

ACTION26.ACTIVE

40125

Unsigned8

Read/Write

-

ACTION27.ACTIVE

40126

Unsigned8

Read/Write

-

ACTION28.ACTIVE

40127

Unsigned8

Read/Write

-

ACTION29.ACTIVE

40128

Unsigned8

Read/Write

-

ACTION30.ACTIVE

40129

Unsigned8

Read/Write

-

ACTION31.ACTIVE

40130

Unsigned8

Read/Write

-

ACTION32.ACTIVE

40131

Unsigned8

Read/Write

-