ACTION#.RUNCOUNT

Description

This keyword displays the number of times an action ran since the time the Action was activated. It does not take any arguments. When an Action is activated, it automatically clears this count. The count value is only available for edge-triggered tasks and not for continuous tasks.

Examples

Code

--> ACTION1.ACTIVE 1
--> ACTION1.RUNCOUNT
0  

Context

See Actions Table.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

N/A

Range

N/A

Default Value

0

Data Type

Integer

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

ACTION1.RUNCOUNT

3903h

01h

Unsigned32

-

-

Read only

No

ACTION2.RUNCOUNT

3903h

02h

Unsigned32

-

-

Read only

No

ACTION3.RUNCOUNT

3903h

03h

Unsigned32

-

-

Read only

No

ACTION4.RUNCOUNT

3903h

04h

Unsigned32

-

-

Read only

No

ACTION5.RUNCOUNT

3903h

05h

Unsigned32

-

-

Read only

No

ACTION6.RUNCOUNT

3903h

06h

Unsigned32

-

-

Read only

No

ACTION7.RUNCOUNT

3903h

07h

Unsigned32

-

-

Read only

No

ACTION8.RUNCOUNT

3903h

08h

Unsigned32

-

-

Read only

No

ACTION9.RUNCOUNT

3903h

09h

Unsigned32

-

-

Read only

No

ACTION10.RUNCOUNT

3903h

0ah

Unsigned32

-

-

Read only

No

ACTION11.RUNCOUNT

3903h

0bh

Unsigned32

-

-

Read only

No

ACTION12.RUNCOUNT

3903h

0ch

Unsigned32

-

-

Read only

No

ACTION13.RUNCOUNT

3903h

0dh

Unsigned32

-

-

Read only

No

ACTION14.RUNCOUNT

3903h

0eh

Unsigned32

-

-

Read only

No

ACTION15.RUNCOUNT

3903h

0fh

Unsigned32

-

-

Read only

No

ACTION16.RUNCOUNT

3903h

10h

Unsigned32

-

-

Read only

No

ACTION17.RUNCOUNT

3903h

11h

Unsigned32

-

-

Read only

No

ACTION18.RUNCOUNT

3903h

12h

Unsigned32

-

-

Read only

No

ACTION19.RUNCOUNT

3903h

13h

Unsigned32

-

-

Read only

No

ACTION20.RUNCOUNT

3903h

14h

Unsigned32

-

-

Read only

No

ACTION21.RUNCOUNT

3903h

15h

Unsigned32

-

-

Read only

No

ACTION22.RUNCOUNT

3903h

16h

Unsigned32

-

-

Read only

No

ACTION23.RUNCOUNT

3903h

17h

Unsigned32

-

-

Read only

No

ACTION24.RUNCOUNT

3903h

18h

Unsigned32

-

-

Read only

No

ACTION25.RUNCOUNT

3903h

19h

Unsigned32

-

-

Read only

No

ACTION26.RUNCOUNT

3903h

1ah

Unsigned32

-

-

Read only

No

ACTION27.RUNCOUNT

3903h

1bh

Unsigned32

-

-

Read only

No

ACTION28.RUNCOUNT

3903h

1ch

Unsigned32

-

-

Read only

No

ACTION29.RUNCOUNT

3903h

1dh

Unsigned32

-

-

Read only

No

ACTION30.RUNCOUNT

3903h

1eh

Unsigned32

-

-

Read only

No

ACTION31.RUNCOUNT

3903h

1fh

Unsigned32

-

-

Read only

No

ACTION32.RUNCOUNT

3903h

20h

Unsigned32

-

-

Read only

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

ACTION1.RUNCOUNT

40400

9DD0

Unsigned32

Read Only

-

ACTION2.RUNCOUNT

40401

9DD1

Unsigned32

Read Only

-

ACTION3.RUNCOUNT

40402

9DD2

Unsigned32

Read Only

-

ACTION4.RUNCOUNT

40403

9DD3

Unsigned32

Read Only

-

ACTION5.RUNCOUNT

40404

9DD4

Unsigned32

Read Only

-

ACTION6.RUNCOUNT

40405

9DD5

Unsigned32

Read Only

-

ACTION7.RUNCOUNT

40406

9DD6

Unsigned32

Read Only

-

ACTION8.RUNCOUNT

40407

9DD7

Unsigned32

Read Only

-

ACTION9.RUNCOUNT

40408

9DD8

Unsigned32

Read Only

-

ACTION10.RUNCOUNT

40409

9DD9

Unsigned32

Read Only

-

ACTION11.RUNCOUNT

40410

9DDA

Unsigned32

Read Only

-

ACTION12.RUNCOUNT

40411

9DDB

Unsigned32

Read Only

-

ACTION13.RUNCOUNT

40412

9DDC

Unsigned32

Read Only

-

ACTION14.RUNCOUNT

40413

9DDD

Unsigned32

Read Only

-

ACTION15.RUNCOUNT

40414

9DDE

Unsigned32

Read Only

-

ACTION16.RUNCOUNT

40415

9DDF

Unsigned32

Read Only

-

ACTION17.RUNCOUNT

40416

9DE0

Unsigned32

Read Only

-

ACTION18.RUNCOUNT

40417

9DE1

Unsigned32

Read Only

-

ACTION19.RUNCOUNT

40418

9DE2

Unsigned32

Read Only

-

ACTION20.RUNCOUNT

40419

9DE3

Unsigned32

Read Only

-

ACTION21.RUNCOUNT

40420

9DE4

Unsigned32

Read Only

-

ACTION22.RUNCOUNT

40421

9DE5

Unsigned32

Read Only

-

ACTION23.RUNCOUNT

40422

9DE6

Unsigned32

Read Only

-

ACTION24.RUNCOUNT

40423

9DE7

Unsigned32

Read Only

-

ACTION25.RUNCOUNT

40424

9DE8

Unsigned32

Read Only

-

ACTION26.RUNCOUNT

40425

9DE9

Unsigned32

Read Only

-

ACTION27.RUNCOUNT

40426

9DEA

Unsigned32

Read Only

-

ACTION28.RUNCOUNT

40427

9DEB

Unsigned32

Read Only

-

ACTION29.RUNCOUNT

40428

9DEC

Unsigned32

Read Only

-

ACTION30.RUNCOUNT

40429

9DED

Unsigned32

Read Only

-

ACTION31.RUNCOUNT

40430

9DEE

Unsigned32

Read Only

-

ACTION32.RUNCOUNT

40431

9DEF

Unsigned32

Read Only

-

PROFINET

Parameter

PNU

Data Type

Access

Units

ACTION1.RUNCOUNT

40400

Unsigned32

Read Only

-

ACTION2.RUNCOUNT

40401

Unsigned32

Read Only

-

ACTION3.RUNCOUNT

40402

Unsigned32

Read Only

-

ACTION4.RUNCOUNT

40403

Unsigned32

Read Only

-

ACTION5.RUNCOUNT

40404

Unsigned32

Read Only

-

ACTION6.RUNCOUNT

40405

Unsigned32

Read Only

-

ACTION7.RUNCOUNT

40406

Unsigned32

Read Only

-

ACTION8.RUNCOUNT

40407

Unsigned32

Read Only

-

ACTION9.RUNCOUNT

40408

Unsigned32

Read Only

-

ACTION10.RUNCOUNT

40409

Unsigned32

Read Only

-

ACTION11.RUNCOUNT

40410

Unsigned32

Read Only

-

ACTION12.RUNCOUNT

40411

Unsigned32

Read Only

-

ACTION13.RUNCOUNT

40412

Unsigned32

Read Only

-

ACTION14.RUNCOUNT

40413

Unsigned32

Read Only

-

ACTION15.RUNCOUNT

40414

Unsigned32

Read Only

-

ACTION16.RUNCOUNT

40415

Unsigned32

Read Only

-

ACTION17.RUNCOUNT

40416

Unsigned32

Read Only

-

ACTION18.RUNCOUNT

40417

Unsigned32

Read Only

-

ACTION19.RUNCOUNT

40418

Unsigned32

Read Only

-

ACTION20.RUNCOUNT

40419

Unsigned32

Read Only

-

ACTION21.RUNCOUNT

40420

Unsigned32

Read Only

-

ACTION22.RUNCOUNT

40421

Unsigned32

Read Only

-

ACTION23.RUNCOUNT

40422

Unsigned32

Read Only

-

ACTION24.RUNCOUNT

40423

Unsigned32

Read Only

-

ACTION25.RUNCOUNT

40424

Unsigned32

Read Only

-

ACTION26.RUNCOUNT

40425

Unsigned32

Read Only

-

ACTION27.RUNCOUNT

40426

Unsigned32

Read Only

-

ACTION28.RUNCOUNT

40427

Unsigned32

Read Only

-

ACTION29.RUNCOUNT

40428

Unsigned32

Read Only

-

ACTION30.RUNCOUNT

40429

Unsigned32

Read Only

-

ACTION31.RUNCOUNT

40430

Unsigned32

Read Only

-

ACTION32.RUNCOUNT

40431

Unsigned32

Read Only

-