AIN#.VALUE
Description
AIN#.VALUE reads the analog input value after the value is filtered (as shown in the Analog Input Block Diagram).
Examples
Code
--> AIN1.VALUE 1.420 V
Context
For more information see Analog Input.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type | Read Only |
Units | V |
Range | -12.5V to +12.5V |
Default Value | N/A |
Data Type | Float |
See Also | |
Stored in Non-Volatile Memory | No |
Variants Supported
All variants are supported.
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
---|---|---|---|---|---|---|---|
AIN1.VALUE |
3780h |
01h |
Signed16 |
- |
1000:1 |
Read only |
Yes |
AIN2.VALUE |
3781h |
01h |
Signed16 |
- |
1000:1 |
Read only |
Yes |
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
---|---|---|---|---|---|---|
23100 |
1 |
23100 (0x5a3c) |
AIN1.VALUE |
Signed16 |
Read Only |
Yes |
23101 |
1 |
23101 (0x5a3d) |
AIN2.VALUE |
Signed16 |
Read Only |
Yes |
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
AIN1.VALUE |
23100 |
Float |
Read Only |
- |
AIN2.VALUE |
23101 |
Float |
Read Only |
- |