AXIS#.IL.AINSOURCE

Description

This parameter sets which analog input to use for AXIS#.IL.AINSCALE.

Value Description
0 Uses no analog input. The current command in analog torque mode is 0.
1 Uses AIN1
2 Uses AIN2

Versions

Action Version Notes
Implemented 02-00-00-000
Added value '0' to range 02-07-02-000  

General Information

Type

Read/Write

Units

N/A

Range

0 to 2

Default Value

0

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.IL.AINSOURCE

500ah

15h

Unsigned8

-

-

Read/Write

No

AXIS2.IL.AINSOURCE

510ah

15h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5811

1

5811 (0x16b3)

AXIS1.IL.AINSOURCE

Unsigned8

Read/Write

Yes

71347

2

5811 (0x16b3)

AXIS2.IL.AINSOURCE

Unsigned8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.IL.AINSOURCE

5811

Unsigned8

Read/Write

-