AXIS#.IL.BW
Description
This parameter sets the current loop bandwidth. The default value is determined by the PWM frequency of the drive and the maximum recommended bandwidth.
The current loop gain AXIS#.IL.KP is calculated as follows:
AXIS#.IL.KP = 2 * pi * AXIS#.MOTOR.LQLL * AXIS#.IL.BW
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
kHz |
Range |
0 to 5 |
Default Value |
Determined by PWM frequency and maximum recommended bandwidth. |
Data Type |
Float |
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
---|---|---|---|---|---|---|---|
AXIS1.IL.BW |
500ah |
16h |
Unsigned16 |
- |
1000:1 |
Read/Write |
No |
AXIS2.IL.BW |
510ah |
16h |
Unsigned16 |
- |
1000:1 |
Read/Write |
No |
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
---|---|---|---|---|---|---|
5818 |
1 |
5818 (0x16ba) |
AXIS1.IL.BW |
Unsigned16 |
Read/Write |
Yes |
71354 |
2 |
5818 (0x16ba) |
AXIS2.IL.BW |
Unsigned16 |
Read/Write |
Yes |
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
AXIS#.IL.BW |
5818 |
Float |
Read/Write |
- |