AXIS#.MOTOR.IMID

Description

This parameter is the preset rotor flux building current for closed loop induction motor control (AXIS#.MOTOR.TYPE = 4).

The value of AXIS#.IL.IMID can be estimated using the motor name plate information.

The following rule should generally be used:

Id root-mean-square approximately equals lr multiplied by the square root of 1 minus open parentheses cos phi close parentheses squared multiplied by 0.8

In which Id is the value for AXIS#.IL.IMID, the preset rotor flux building current, Ir is the name plate phase current, cosϕ is the name plate power factor at rated and operation, and 0.8 is an empirical factor (accounts for the angle error due to voltage drop on the leakage induction).


  • This parameter is required to be configured for AXIS#.MOTOR.TYPE = 4

Context

For more information see Motor.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Arms

Range

0 to DRIVE.IPEAK

Default Value

0

Data Type

Float

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.MOTOR.IMID

500bh

0ah

Unsigned16

-

1000:1

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6229

1

6229 (0x1855)

AXIS1.MOTOR.IMID

Unsigned16

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.MOTOR.IMID

6229

Float

Read/Write

-