AXIS#.MOTOR.LQLL
Description
This parameter is the motor line-to-line quadrature (torque producing) axis inductance.
-
- This parameter is automatically configured for Kollmorgen motors when AXIS#.MOTOR.AUTOSET = 1 and can be modified while AXIS#.MOTOR.AUTOSET = 1 if its AXIS#.MOTOR.DISAUTOSET index = 1.
-
-
This parameter is required to be configured for AXIS#.MOTOR.TYPE = 0, 1, 4, 6, and 8.
Context
For more information see Motor.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
mH |
Range |
1 to 232 mH |
Default Value |
4 |
Data Type |
Float |
See Also |
N/A |
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
---|---|---|---|---|---|---|---|
AXIS1.MOTOR.LQLL |
500bh |
14h |
Unsigned32 |
- |
1000:1 |
Read/Write |
No |
AXIS2.MOTOR.LQLL |
510bh |
14h |
Unsigned32 |
- |
1000:1 |
Read/Write |
No |
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
---|---|---|---|---|---|---|
6209 |
1 |
6209 (0x1841) |
AXIS1.MOTOR.LQLL |
Unsigned32 |
Read Only |
Yes |
71745 |
2 |
6209 (0x1841) |
AXIS2.MOTOR.LQLL |
Unsigned32 |
Read Only |
Yes |
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
AXIS#.MOTOR.LQLL |
6209 |
Float |
Read Only |
- |