AXIS#.MOTOR.PITCH
Description
This parameter is used with linear encoders. It defines a distance in millimeters which is determined by how the linear enocoder is used.
-
When used with a linear motor, it defines the pole-to-pole pitch. The pitch is the distance between two similar poles. Kollmorgen linear motors have a pitch of 32mm.
-
When using a linear encoder in a dual loop configuration in which the linear encoder is used as a secondary position feedback, the distance specified is equal to the distance the linear encoder travels given one rotation of the rotary motor.
-
-
This parameter is required to be configured for AXIS#.MOTOR.TYPE = 1 or when using a linear encoder as the AXIS#.PL.FBSOURCE.
Context
For more information see Motor.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 | |
Added dual loop behavior | 02-09-03-000 | AXIS#.MOTOR.PITCH was not previously included in the resolution calculation when using a linear encoder only as a position source. In order to relate the rotary motor with the linear encoder for proper control, this parameter is now required to be set. |
General Information
Type |
Read/Write |
Units |
mm |
Range |
0.001 to 1000 |
Default Value |
32 |
Data Type |
Float |
See Also |
N/A |
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
---|---|---|---|---|---|---|---|
AXIS1.MOTOR.PITCH |
500bh |
16h |
Unsigned32 |
- |
1000:1 |
Read/Write |
No |
AXIS2.MOTOR.PITCH |
510bh |
16h |
Unsigned32 |
- |
1000:1 |
Read/Write |
No |
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
---|---|---|---|---|---|---|
6211 |
1 |
6211 (0x1843) |
AXIS1.MOTOR.PITCH |
Unsigned32 |
Read/Write |
Yes |
71747 |
2 |
6211 (0x1843) |
AXIS2.MOTOR.PITCH |
Unsigned32 |
Read/Write |
Yes |
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
AXIS#.MOTOR.PITCH |
6211 |
Float |
Read/Write |
- |