AXIS#.MOTOR.VOLTRATED
Description
This parameter configures the drive for the induction motor's rated voltage as indicated on the nameplate.
AXIS#.MOTOR.VOLTRATED is used to calculate the constant Volts per Hertz characteristics of the drive and motor.
-
-
This parameter is required to be configured for AXIS#.MOTOR.TYPE = 2.
Context
For more information see Motor.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
V |
Range |
50 to 1,000 V |
Default Value |
230 V |
Data Type |
Integer |
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
---|---|---|---|---|---|---|---|
AXIS1.MOTOR.VOLTRATED |
500bh |
06h |
Unsigned16 |
- |
- |
Read/Write |
No |
AXIS2.MOTOR.VOLTRATED |
510bh |
06h |
Unsigned16 |
- |
- |
Read/Write |
No |
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
---|---|---|---|---|---|---|
6226 |
1 |
6226 (0x1852) |
AXIS1.MOTOR.VOLTRATED |
Unsigned16 |
Read/Write |
Yes |
71762 |
2 |
6226 (0x1852) |
AXIS2.MOTOR.VOLTRATED |
Unsigned16 |
Read/Write |
Yes |
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
AXIS#.MOTOR.VOLTRATED |
6226 |
Unsigned16 |
Read/Write |
- |