AXIS#.VL.ACCFILTERED

Description

AXIS#.VL.ACCFILTERED returns the filtered acceleration.

Versions

Action Version Notes
Implemented 02-04-01-000

 

General Information

Type

Read Only

Description Depends on AXIS#.UNIT.ACCROTARY
Units

Rotary: RPM/s, RPS/s, deg/s2, (custom units)/s2, rad/s2

Range

N/A

Default Value

N/A

Data Type

Float

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Fieldbus Information

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6041

1

6041 (0x1799)

AXIS1.VL.ACCFILTERED

Signed32

Read Only

Yes

71577

2

6041 (0x1799)

AXIS2.VL.ACCFILTERED

Signed32

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.VL.ACCFILTERED

6041

Float

Read Only

Acceleration

Related Topics

Velocity Loop