AXIS#.WS.DISTMIN
Description
This parameter sets the minimum movement that is required for commutation finding. If this value is too small, then the commutation finding might fail if too little current is used. The larger this value, the more movement is needed in order to avoid F5500: "Wake and Shake - Insufficient movement".
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
Actual position units |
Range |
0 to 90 deg |
Default Value |
1 deg |
Data Type |
Float |
See Also |
N/A |
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
---|---|---|---|---|---|---|---|
AXIS1.WS.DISTMIN |
5013h |
0fh |
Signed32 |
Position |
- |
Read/Write |
No |
AXIS2.WS.DISTMIN |
5113h |
0fh |
Signed32 |
Position |
- |
Read/Write |
No |
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
---|---|---|---|---|---|---|
6702 |
1 |
6702 (0x1a2e) |
AXIS1.WS.DISTMIN |
Signed32 |
Read/Write |
Yes |
72238 |
2 |
6702 (0x1a2e) |
AXIS2.WS.DISTMIN |
Signed32 |
Read/Write |
Yes |
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
AXIS#.WS.DISTMIN |
6702 |
Signed32 |
Read/Write |
Position |