AXIS#.WS.FREQ

Description

This keyword sets the excitation frequency for Wake and Shake mode 2.

The default setting of 10Hz will work for almost all systems.

In cases where the load attached to the motor is much higher than the motor inertia (200:1) it may be necessary to lower the value of AXIS#.WS.FREQ.

Effects of lowering AXIS#.WS.FREQ:

  • Wake and Shake Mode 2 will take longer to complete.
  • A higher magnitude of motion will be seen on the motor because the motor has current applied in the same direction for a longer period of time.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Hz

Range

0.01 - 8000

Default Value

10

Data Type

Float

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.WS.FREQ

5013h

13h

Unsigned32

-

1000:1

Read/Write

No

AXIS2.WS.FREQ

5113h

13h

Unsigned32

-

1000:1

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6713

1

6713 (0x1a39)

AXIS1.WS.FREQ

Unsigned32

Read/Write

Yes

72249

2

6713 (0x1a39)

AXIS2.WS.FREQ

Unsigned32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.WS.FREQ

6713

Float

Read/Write

-

Related Topics

AXIS#.WS.MODE