AXIS#.ZEROACC

Description

AXIS#.ZEROACC is the acceleration threshold for the motor to be considered at zero velocity.

If AXIS#.ZEROACC is equal to 0, acceleration will not be included in determining zero velocity. If AXIS#.ZEROACC is greater than zero, it will be included.

Versions

Action Version Notes
Implemented 02-04-01-000

 

General Information

Type

Read/Write

Units

Rotary: RPM/s, RPS/s, deg/s2, (custom units)/s2, rad/s2

Linear: counts/s2, mm/s2, µm/s2, (custom units)/s2

See Acceleration Units for details.

Range

Depends on units. See Acceleration Range for details.

Default Value

0 RPM

Depends on units. See Acceleration Units for details.

Data Type

Float

Stored in Non Volatile Memory Yes

Variants Supported

All variants supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.ZEROACC

5002h

05h

Unsigned32

Acceleration

-

Read/Write

No

AXIS2.ZEROACC

5102h

05h

Unsigned32

Acceleration

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5031

1

5031 (0x13a7)

AXIS1.ZEROACC

Unsigned32

Read/Write

Yes

70567

2

5031 (0x13a7)

AXIS2.ZEROACC

Unsigned32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.ZEROACC

5031

Float

Read/Write

Acceleration