BRAKE#.AXIS

Description

Sets which axis will control the brake.

Value Description
0 Not used
1 Controlled by Axis 1.
2 Controlled by Axis 2.

Examples

Context

For more information see Brake.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 2

Default Value

Depends on Brake and Axis number:

BRAKE1 defaults to 1.

BRAKE2 defaults to 2 on multi-axis drives and 0 on single-axis drives.

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

BRAKE1.AXIS

3012h

01h

Unsigned8

-

-

Read/Write

No

BRAKE2.AXIS

3012h

02h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

3100

1

3100 (0xc1c)

BRAKE1.AXIS

Unsigned8

Read/Write

Yes

3101

1

3101 (0xc1d)

BRAKE2.AXIS

Unsigned8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

BRAKE1.AXIS

3100

Unsigned8

Read/Write

-

BRAKE2.AXIS

3101

Unsigned8

Read/Write

-