BRAKE#.STATE

Description

Reads whether the brake is released or applied.

Value Description
0 Brake applied
1 Brake released

Examples

Context

For more information see Brake.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Integer

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Fieldbus Information

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

3105

1

3105 (0xc21)

BRAKE1.STATE

Unsigned8

Read Only

Yes

3106

1

3106 (0xc22)

BRAKE2.STATE

Unsigned8

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

BRAKE1.STATE

3105

Unsigned8

Read Only

-

BRAKE2.STATE

3106

Unsigned8

Read Only

-