CMP#.MODEN

Description

CMP#.MODEN turns the modulo function for the compare channel on or off.

Examples

Usage

0: Turn modulo off (default)

1: Turn modulo on

Code

The following commands turn modulo on for channel 1 and off for channel 2.

--> CMP1.MODEN 1
--> CMP2.MODEN 0

Context

For more information please refer to Compare.

Versions

Action Version Notes
Implemented 02-06-00-000  

General Information

Type

Read/Write

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Integer

See Also

CMP#.MODVAL1, CMP#.MODVAL2

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

CMP1.MODEN

4500h

02h

Unsigned8

-

-

Read/Write

No

CMP2.MODEN

4501h

02h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

31520

1

31520 (0x7b20)

CMP1.MODEN

Unsigned8

Read/Write

Yes

31521

1

31521 (0x7b21)

CMP2.MODEN

Unsigned8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

CMP1.MODEN

31520

Unsigned8

Read/Write

-

CMP2.MODEN

31521

Unsigned8

Read/Write

-