CMP#.SOURCEVAL

Description

CMP#.SOURCEVAL is the sampled value of the compare channel source. It reports the value before the channel’s modulo function is applied if CMP#.MODEN = 1. Its scaling depends on CMP#.SOURCE.

  CMP#.MODEN
0 1
CMP#.SOURCE 1-10

FB#.P without modification

FB#.P with modulo

11-12

AXIS#.PL.FB without modification

AXIS#.PL.FB with modulo

Examples

Usage

Code

These commands read the values for channel 1 and channel 2. In this example the units for CMP1.SOURCEVAL are deg, and the units of CMP2.SOURCEVAL are feedback counts.

--> CMP1.SOURCE 12
--> AXIS1.UNIT.PROTARY 2
--> CMP1.SOURCEVAL
-749.205
--> CMP2.SOURCE 3
--> CMP2.SOURCEVAL
493626.000

Context

See Compare Engines View.

Versions

Action Version Notes
Implemented 02-06-00-000  

General Information

Type

Read Only

Units

Depends upon CMP#.SOURCE

Range

Full Position Range

Default Value

N/A

Data Type

Float

See Also

 

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

CMP1.SOURCEVAL

4500h

04h

Signed32

-

1000:1

Read only

No

CMP2.SOURCEVAL

4501h

04h

Signed32

-

1000:1

Read only

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

31600

1

31600 (0x7b70)

CMP1.SOURCEVAL

Signed32

Read Only

Yes

31601

1

31601 (0x7b71)

CMP2.SOURCEVAL

Signed32

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

CMP1.SOURCEVAL

31600

Signed32

Read Only

Position

CMP2.SOURCEVAL

31601

Signed32

Read Only

Position