DIN#.STATE

Description

Reads the state of one digital input according to the number identified in the command.

Examples

Code

--> DIN1.STATE
1

Context

For more information see Digital Inputs and Outputs.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read Only
Units N/A
Range 0 to 1
Default Value N/A
Data Type Integer
See Also  

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Fieldbus Information

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

20000

1

20000 (0x4e20)

DIN1.STATE

Unsigned8

Read Only

Yes

20001

1

20001 (0x4e21)

DIN2.STATE

Unsigned8

Read Only

Yes

20002

1

20002 (0x4e22)

DIN3.STATE

Unsigned8

Read Only

Yes

20003

1

20003 (0x4e23)

DIN4.STATE

Unsigned8

Read Only

Yes

20004

1

20004 (0x4e24)

DIN5.STATE

Unsigned8

Read Only

Yes

20005

1

20005 (0x4e25)

DIN6.STATE

Unsigned8

Read Only

Yes

20006

1

20006 (0x4e26)

DIN7.STATE

Unsigned8

Read Only

Yes

20007

1

20007 (0x4e27)

DIN8.STATE

Unsigned8

Read Only

Yes

20008

1

20008 (0x4e28)

DIN9.STATE

Unsigned8

Read Only

Yes

20009

1

20009 (0x4e29)

DIN10.STATE

Unsigned8

Read Only

Yes

20010

1

20010 (0x4e2a)

DIN11.STATE

Unsigned8

Read Only

Yes

20011

1

20011 (0x4e2b)

DIN12.STATE

Unsigned8

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

DIN1.STATE

20000

Unsigned8

Read Only

-

DIN2.STATE

20001

Unsigned8

Read Only

-

DIN3.STATE

20002

Unsigned8

Read Only

-

DIN4.STATE

20003

Unsigned8

Read Only

-

DIN5.STATE

20004

Unsigned8

Read Only

-

DIN6.STATE

20005

Unsigned8

Read Only

-

DIN7.STATE

20006

Unsigned8

Read Only

-

DIN8.STATE

20007

Unsigned8

Read Only

-

DIN9.STATE

20008

Unsigned8

Read Only

-

DIN10.STATE

20009

Unsigned8

Read Only

-

DIN11.STATE

20010

Unsigned8

Read Only

-

DIN12.STATE

20011

Unsigned8

Read Only

-