DIO#.DIR
Description
Sets or whether the bi-directional IO is an input or output.
| Value | Description |
|---|---|
| 0 | The bi-directional IO is treated as an input signal |
| 1 | The bi-directional IO is treated as an output signal |
Examples
Context
For more information see Digital Inputs and Outputs.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
| Type | Read/Write |
| Units | N/A |
| Range | 0 to 1 |
| Default Value | 0 (input) |
| Data Type | Integer |
| See Also | |
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
DIO1.DIR |
368ah |
01h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
DIO2.DIR |
368bh |
01h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
DIO3.DIR |
368ch |
01h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
DIO4.DIR |
368dh |
01h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
DIO5.DIR |
368eh |
01h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
DIO6.DIR |
368fh |
01h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
22050 |
1 |
22050 (0x5622) |
DIO1.DIR |
Unsigned8 |
Read/Write |
Yes |
|
22051 |
1 |
22051 (0x5623) |
DIO2.DIR |
Unsigned8 |
Read/Write |
Yes |
|
22052 |
1 |
22052 (0x5624) |
DIO3.DIR |
Unsigned8 |
Read/Write |
Yes |
|
22053 |
1 |
22053 (0x5625) |
DIO4.DIR |
Unsigned8 |
Read/Write |
Yes |
|
22054 |
1 |
22054 (0x5626) |
DIO5.DIR |
Unsigned8 |
Read/Write |
Yes |
|
22055 |
1 |
22055 (0x5627) |
DIO6.DIR |
Unsigned8 |
Read/Write |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
DIO1.DIR |
22050 |
Unsigned8 |
Read/Write |
- |
|
DIO2.DIR |
22051 |
Unsigned8 |
Read/Write |
- |
|
DIO3.DIR |
22052 |
Unsigned8 |
Read/Write |
- |
|
DIO4.DIR |
22053 |
Unsigned8 |
Read/Write |
- |
|
DIO5.DIR |
22054 |
Unsigned8 |
Read/Write |
- |
|
DIO6.DIR |
22055 |
Unsigned8 |
Read/Write |
- |