DIO#.SOURCEID

Description

DIO#.SOURCEID sets the digital I/O source ID, for sources that require an ID.

Examples

Usage

DIO#.SOURCEID can be used to select the compare channel whenDIO#.SOURCE = 4 (Compare).

Code

The following commands set the source of digital IO 1 to compare channel 1, and digital IO 2 to compare channel 2.

--> DIO1.SOURCE 4
--> DIO1.SOURCEID 1
--> DIO2.SOURCE 4
--> DIO2.SOURCEID 2

Context

For more information see Digital Inputs and Outputs.

Versions

Action Version Notes
Implemented 02-00-00-000  
Added Compare source 02-06-00-000  

General Information

Type Read/Write
Units N/A
Range 1 to 2
Default Value 0
Data Type Integer
See Also  

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

DIO1.SOURCEID

368ah

06h

Unsigned8

-

-

Read/Write

No

DIO2.SOURCEID

368bh

06h

Unsigned8

-

-

Read/Write

No

DIO3.SOURCEID

368ch

06h

Unsigned8

-

-

Read/Write

No

DIO4.SOURCEID

368dh

06h

Unsigned8

-

-

Read/Write

No

DIO5.SOURCEID

368eh

06h

Unsigned8

-

-

Read/Write

No

DIO6.SOURCEID

368fh

06h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

22300

1

22300 (0x571c)

DIO1.SOURCEID

Unsigned8

Read/Write

Yes

22301

1

22301 (0x571d)

DIO2.SOURCEID

Unsigned8

Read/Write

Yes

22302

1

22302 (0x571e)

DIO3.SOURCEID

Unsigned8

Read/Write

Yes

22303

1

22303 (0x571f)

DIO4.SOURCEID

Unsigned8

Read/Write

Yes

22304

1

22304 (0x5720)

DIO5.SOURCEID

Unsigned8

Read/Write

Yes

22305

1

22305 (0x5721)

DIO6.SOURCEID

Unsigned8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

DIO1.SOURCEID

22300

Unsigned8

Read/Write

-

DIO2.SOURCEID

22301

Unsigned8

Read/Write

-

DIO3.SOURCEID

22302

Unsigned8

Read/Write

-

DIO4.SOURCEID

22303

Unsigned8

Read/Write

-

DIO5.SOURCEID

22304

Unsigned8

Read/Write

-

DIO6.SOURCEID

22305

Unsigned8

Read/Write

-