DRV.CPUPERCENT

Description

DRV.CPUPERCENT returns a percentage representing the execution time of the 16kHz loop versus the total 16kHz period (62.5us).

This keyword can be used to approximate the load on the drive’s processor.


  • If this value exceeds 75%, F3008 will occur.
Parameter Value Drive Action
0 Disable Amplifier
1 Ignore. Fault will not be reported.

General Information

Type Read Only
Units Percent
Range N/A
Default Value N/A
Data Type Float

Stored in Non-Volatile Memory

No

Variants Supported

AKD2G

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

DRV.CPUPERCENT

3000h

0ah

Unsigned16

-

-

Read only

Yes

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

2024

1

2024 (0x7e8)

DRV.CPUPERCENT

Unsigned16

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

DRV.CPUPERCENT

2024

Float

Read Only

-