DRV.NVLOAD
Description
DRV.NVLOAD loads all data from the NV memory of the drive into the RAM parameters.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Command |
Units |
N/A |
Range |
N/A |
Default Value |
N/A |
Data Type |
N/A |
Stored in Non-Volatile Memory |
No |
Variants Supported
All variants are supported.
Fieldbus Information
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
---|---|---|---|---|---|---|
2007 |
1 |
2007 (0x7d7) |
DRV.NVLOAD |
Unsigned8 |
Read/Write |
No |
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
DRV.NVLOAD |
2007 |
Unsigned8 |
Read/Write |
- |