DRV.RECPRMLIST

Description

This command returns the list of recordable parameters. You can use a recordable parameter as an input to any of the recording channels.



  • An internal address or a registered variable can be used as input to any of the channels in addition to the list.

Examples

Code

-->DRV.RECPRMLIST
AIN1.VALUE
AIN2.VALUE
AOUT1.VALUE
AOUT1.VALUEU
AOUT2.VALUE
AOUT2.VALUEU
AXIS1.ACTIVE
...

Context

For more information see Scope.

Versions

Action Version Notes
Implemented 02-10-00-000

General Information

Variants Supported

All variants are supported.