EEO#.PIN

Description

EEO#.PIN is used in conjunction with EEO#.POUT to set the gain of the EEO position going to the EEO Generator. The maximum value of EEO#.PIN / EEO#.POUT is 32.

Versions

Action Version Notes
Implemented 02-07-00-000

General Information

Type Read/Write
Description Sets the gear IN of the EEO position
Units N/A
Range 1 to 4,294,967,295
Default Value 1
Data Type Integer
See Also EEO#.POUT
Stored in Non-Volatile Memory Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

EEO1.PIN

4600h

08h

Unsigned32

-

-

Read/Write

No

EEO2.PIN

4601h

08h

Unsigned32

-

-

Read/Write

No

EEO3.PIN

4603h

08h

Unsigned32

-

-

Read/Write

No

EEO4.PIN

4606h

08h

Unsigned32

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

32045

1

32045 (0x7d2d)

EEO1.PIN

Unsigned32

Read/Write

Yes

32046

1

32046 (0x7d2e)

EEO2.PIN

Unsigned32

Read/Write

Yes

32047

1

32047 (0x7d2f)

EEO3.PIN

Unsigned32

Read/Write

Yes

32048

1

32048 (0x7d30)

EEO4.PIN

Unsigned32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

EEO1.PIN

32045

Unsigned32

Read/Write

-

EEO2.PIN

32046

Unsigned32

Read/Write

-

EEO3.PIN

32047

Unsigned32

Read/Write

-

EEO4.PIN

32048

Unsigned32

Read/Write

-