FB#.STOREMULTITURN.ENABLE

Description

This keyword enables or disables the store multiturn feature.

To prevent rollovers, set FB#.STOREMULTITURN.ENABLE = 1. Whenever the drive is power cycled after passing multiturn rollovers, the drive will keep track of the rollovers and retain the correct position.

Enabled  
0 (default) Disabled
1 Enabled

Context

See Store Multiturn

Versions

Action

Version

Notes

Implemented

02-08-03-000

General Information

Type

Read/Write

Units

N/A

Range

0, 1

Default Value

0

Data Type

Integer

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

FB1.STOREMULTITURN.ENABLE

3500h

0fh

Unsigned8

-

-

Read/Write

No

FB2.STOREMULTITURN.ENABLE

3501h

0fh

Unsigned8

-

-

Read/Write

No

FB3.STOREMULTITURN.ENABLE

3502h

0fh

Unsigned8

-

-

Read/Write

No

FB4.STOREMULTITURN.ENABLE

3503h

0fh

Unsigned8

-

-

Read/Write

No

FB5.STOREMULTITURN.ENABLE

3504h

0fh

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

30460

1

30460 (0x76fc)

FB1.STOREMULTITURN.ENABLE

Unsigned8

Read/Write

Yes

30461

1

30461 (0x76fd)

FB2.STOREMULTITURN.ENABLE

Unsigned8

Read/Write

Yes

30462

1

30462 (0x76fe)

FB3.STOREMULTITURN.ENABLE

Unsigned8

Read/Write

Yes

30463

1

30463 (0x76ff)

FB4.STOREMULTITURN.ENABLE

Unsigned8

Read/Write

Yes

30464

1

30464 (0x7700)

FB5.STOREMULTITURN.ENABLE

Unsigned8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

FB1.STOREMULTITURN.ENABLE

30460

Unsigned8

Read/Write

-

FB2.STOREMULTITURN.ENABLE

30461

Unsigned8

Read/Write

-

FB3.STOREMULTITURN.ENABLE

30462

Unsigned8

Read/Write

-

FB4.STOREMULTITURN.ENABLE

30463

Unsigned8

Read/Write

-

FB5.STOREMULTITURN.ENABLE

30464

Unsigned8

Read/Write

-