FB#.MULTITURNBITS

Description

Number of multi-turn bits used for BiSS encoders when used in rotary motors. This is specified by the feedback datasheet.

Context

Only used when FB#.MECHTYPE is rotary and identified feedback is BiSS. See Feedback # View.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

multi-turn bits

Range

0 to 32

Default Value

12

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

FB1.MULTITURNBITS

3500h

0ch

Unsigned8

-

-

Read/Write

No

FB2.MULTITURNBITS

3501h

0ch

Unsigned8

-

-

Read/Write

No

FB3.MULTITURNBITS

3502h

0ch

Unsigned8

-

-

Read/Write

No

FB4.MULTITURNBITS

3503h

0ch

Unsigned8

-

-

Read/Write

No

FB5.MULTITURNBITS

3504h

0ch

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

30340

1

30340 (0x7684)

FB1.MULTITURNBITS

Unsigned8

Read/Write

Yes

30341

1

30341 (0x7685)

FB2.MULTITURNBITS

Unsigned8

Read/Write

Yes

30342

1

30342 (0x7686)

FB3.MULTITURNBITS

Unsigned8

Read/Write

Yes

30343

1

30343 (0x7687)

FB4.MULTITURNBITS

Unsigned8

Read/Write

Yes

30344

1

30344 (0x7688)

FB5.MULTITURNBITS

Unsigned8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

FB1.MULTITURNBITS

30340

Unsigned8

Read/Write

-

FB2.MULTITURNBITS

30341

Unsigned8

Read/Write

-

FB3.MULTITURNBITS

30342

Unsigned8

Read/Write

-

FB4.MULTITURNBITS

30343

Unsigned8

Read/Write

-

FB5.MULTITURNBITS

30344

Unsigned8

Read/Write

-