FB#.SINGLETURNBITS

Description

Number of single turn bits used for BiSS rotary encoders. Feedback data sheet specifies the number required.

Context

Only used for when FB#.MECHTYPE is rotary and identified feedback is BiSS. See Feedback # View.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

single turn bits

Range

1 to 32

Default Value

19

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

FB1.SINGLETURNBITS

3500h

0dh

Unsigned8

-

-

Read/Write

No

FB2.SINGLETURNBITS

3501h

0dh

Unsigned8

-

-

Read/Write

No

FB3.SINGLETURNBITS

3502h

0dh

Unsigned8

-

-

Read/Write

No

FB4.SINGLETURNBITS

3503h

0dh

Unsigned8

-

-

Read/Write

No

FB5.SINGLETURNBITS

3504h

0dh

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

30320

1

30320 (0x7670)

FB1.SINGLETURNBITS

Unsigned8

Read/Write

Yes

30321

1

30321 (0x7671)

FB2.SINGLETURNBITS

Unsigned8

Read/Write

Yes

30322

1

30322 (0x7672)

FB3.SINGLETURNBITS

Unsigned8

Read/Write

Yes

30323

1

30323 (0x7673)

FB4.SINGLETURNBITS

Unsigned8

Read/Write

Yes

30324

1

30324 (0x7674)

FB5.SINGLETURNBITS

Unsigned8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

FB1.SINGLETURNBITS

30320

Unsigned8

Read/Write

-

FB2.SINGLETURNBITS

30321

Unsigned8

Read/Write

-

FB3.SINGLETURNBITS

30322

Unsigned8

Read/Write

-

FB4.SINGLETURNBITS

30323

Unsigned8

Read/Write

-

FB5.SINGLETURNBITS

30324

Unsigned8

Read/Write

-