PWM#.DUTYCYCLE

Description

Sets the duty cycle of the PWM signal, that can be output on a digital IO with DIO#.SOURCE 6.

Versions

Action Version Notes
Implemented 02-11-03-000  

General Information

Type Read/Write
Units Percent
Range 0.0 to 100.0
Default Value 0.0
Data Type Float

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported