REC.ACTIVE
Description
REC.ACTIVE indicates whether or not data recording is in progress. Recording is in progress if the trigger was met and the recorder is recording all data.
Examples
Code
Indicates that recording is not in progress.
-->REC.ACTIVE 0
Context
For more information see Scope.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read Only |
Units |
N/A |
Range |
0 to 1 |
Default Value |
N/A |
Data Type |
Integer |
See Also |
|
Stored in Non-Volatile Memory |
No |
Variants Supported
All variants are supported.
Fieldbus Information
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
---|---|---|---|---|---|---|
2300 |
1 |
2300 (0x8fc) |
REC.ACTIVE |
Unsigned8 |
Read Only |
Yes |
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
REC.ACTIVE |
2300 |
Unsigned8 |
Read Only |
- |