REC.RETRIEVE

Description

REC.RETRIEVE causes the drive to transfer all the recorded data to the communication channel. The data is encoded so that it can be interpreted by WorkBench.

Example

The following code retrieves all data (1000 records in one command).

-->REC.NUMPOINTS 1000
-->REC.TRIG
-->REC.RETRIEVE

Context

For more information see Scope.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

N/A

Range

N/A

Default Value

N/A

Data Type

String

See Also

N/A

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.