REGEN.TYPE
Description
You can specify a user-defined external regen resistor or select the internal regen resistor. The values for REGEN.TYPE are shown below:
Type |
Option |
Description |
---|---|---|
–1 |
External Regen |
External user-defined regen resistor |
0 |
Internal Regen (if available) |
Internal regen resistor |
If a user-defined regen resistor is specified, then you must also define this resistor's resistance (REGEN.REXT ), heatup time (REGEN.TEXT ), and power (REGEN.WATTEXT ).
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
N/A |
Range |
–1 to 0 |
Default Value |
0 |
Data Type |
Integer |
See Also |
N/A |
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
---|---|---|---|---|---|---|---|
REGEN.TYPE |
3007h |
03h |
Signed8 |
- |
- |
Read/Write |
No |
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
---|---|---|---|---|---|---|
2403 |
1 |
2403 (0x963) |
REGEN.TYPE |
Signed8 |
Read/Write |
Yes |
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
REGEN.TYPE |
2403 |
Signed8 |
Read/Write |
- |