VBUS.INRUSHOFF

Description

This parameter returns the voltage at which the DC bus inrush relay opens.

Examples

Usage

The drive configures this parameter based on power electronics component ratings. When the measured DC bus voltage VBUS.VALUE is less than VBUS.INRUSHOFF, the drive opens the inrush relay.

Context

For more information on DC bus operation, refer to Power.

Versions

Action Version Notes
Implemented 02-02-03-000  

General Information

Type

Read Only

Units

VDC

Range

N/A

Default Value

N/A

Data Type

Integer

See Also VBUS.VALUE, VBUS.INRUSHON

Stored in Non-Volatile Memory

No

Variants Supported

All variants supported.

Fieldbus Information

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

2505

1

2505 (0x9c9)

VBUS.INRUSHOFF

Unsigned16

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

VBUS.INRUSHOFF

2505

Unsigned16

Read Only

-