COGCOMP.CORRECTIONTABLE

Description

Reads or writes to the cogging compensation table.

Examples

Reads the full table:

COGCOMP.CORRECTIONTABLE

Reads the compensation value for index "x":

COGCOMP.CORRECTIONTABLE x

Writes the value "y" to the table at index "x":

COGCOMP.CORRECTIONTABLE x y

General Information

This content is not applicable to KAS.

Type

R/W Parameter

Units

mA

Range

Argument 1: 0 to 8,191

Argument 2: 1.628 * DRV.IPEAK

Default Value

0

Data Type

Integer

Start Version

M_01-14-06-001

Variant Supported
MKD EtherCAT Yes
AKD-N Yes
MKD-N Yes
MKD-C No