COGCOMP.RANGELOW

Description

This parameter stores the position of the lower end of the range where cogging compensation is active on a linear axis. On rotary axis, it stores the position of the lower end of the range when the parameter is unequal to 0.

When the value is changed while compensation values are configured, the compensation values will be redistributed over the new range, which will most likely lead to incorrect compensation.

Before starting COGCOMP.TEACH on a linear axis, the value in COGCOMP.RANGELOW has to be smaller than COGCOMP.RANGEHIGH.

General Information

This content is not applicable to KAS.

Type

NV Parameter

Units

Position units

Range

-9,223,372,036,854,774 [counts] to 9,223,372,036,854,774 [counts] or equivalent in position units

Default Value

0

Data Type

Float

Start Version

M_01-14-06-001

Variant Supported
MKD EtherCAT Yes
AKD-N Yes
MKD-N Yes
MKD-C No
EtherCAT CoE and CANopen ]
Index/Subindex Object Start Version

5418h/0

M_01-14-06-001