COGCOMP.V
Description
Velocity for the move during automatic teaching of the cogging compensation table.
General Information
This content is not applicable to KAS.
Type |
NV Parameter |
Units |
Depends on UNIT.VROTARY or UNIT.VLINEAR Rotary: rpm, rps, deg/s, (custom units)/s, rad/s Linear: counts/s, mm/s, µm/s, (custom units)/s |
Range |
N/A |
Default Value |
N/A |
Data Type |
Float |
Start Version |
M_01-14-06-001 |
Variant | Supported |
---|---|
AKD EtherCAT | Yes |
AKD-N | Yes |
AKD-N | Yes |
AKD-C | No |
Index/Subindex | Object Start Version |
---|---|
5414h/0 |
M_01-14-06-001 |