DIN.STATES
Description
DIN.STATES reads the states of the digital inputs.
-
-
AKD-N only supports DIN1 to DIN3.
-
-
AKD-N only supports DIN1 to DIN2.
General Information
|
Type |
R/O Parameter |
|
Units |
N/A |
|
Range |
0000000 to 1111111 |
|
Default Value |
N/A |
|
Data Type |
String |
|
Start Version |
M_01-00-00-000 |
| AKD-N Information | |
|---|---|
| Range | 000 to 111 |
| Variant | Supported |
|---|---|
| MKD EtherCAT | Yes |
| AKD-N | Yes |
| MKD-N | Yes |
| MKD-C | Yes |