MOTOR.ICONT
Description
This parameter is used to configure the motor continuous current.
-
- This parameter is automatically configured for Kollmorgen motors when AXIS#.MOTOR.AUTOSET = 1 and can be modified while AXIS#.MOTOR.AUTOSET = 1 if its AXIS#.MOTOR.DISAUTOSET index = 1.
General Information
|
Type |
NV Parameter |
|
Units |
A |
|
Range |
0.1 to 500 A |
|
Default Value |
1.0 A |
|
Data Type |
Float |
|
See Also |
N/A |
|
Start Version |
M_01-00-00-000 |
|
AKD BASIC Information |
|
|---|---|
|
Type |
R/W |
| Variant | Supported |
|---|---|
| MKD EtherCAT | Yes |
| AKD-N | Yes |
| MKD-N | Yes |
| MKD-C | No |
| Index/Subindex | Object Start Version |
|---|---|
| 358Eh/0 | M_01-00-00-000 |
Related Topics