VBUS.OVFTHRESH

Description

VBUS.OVFTHRESH reads the over voltage fault level for the DC bus.

This value is read from the drive EEPROM and varies according to the drive type.

General Information

Type

R/O Parameter

Units

VDC

Range

0 to 900VDC

Default Value

N/A

Data Type

Integer

See Also

VBUS.UVFTHRESH

Start Version

M_01-00-00-000

Variant Supported
MKD EtherCAT Yes
AKD-N Yes
MKD-N Yes
MKD-C Yes

Related Topics

1   Regeneration