VBUS.OVWTHRESH

Description

If VBUS.VALUE value exceeds VBUS.OVWTHRESH, then a warning is generated. The warning is removed if the voltage returns to below 97% (1/32) of the overvoltage warning level.

General Information

Type

NV Parameter

Units

VDC

Range

0 to 900 VDC

Default Value

0 VDC (warning disabled)

Data Type

U16

See Also

N/A

Start Version

M_01-00-00-000

Variant Supported
MKD EtherCAT Yes
AKD-N Yes
MKD-N Yes
MKD-C Yes
EtherCAT CoE and CANopen
Index/Subindex Object Start Version

518Eh/0

M_01-00-00-000

Related Topics

1   Regeneration