VBUS.UVMODE

Description

This parameter indicates undervoltage (UV) mode.

When VBUS.UVMODE - 0, an undervoltage fault is issued whenever the DC bus goes below the undervoltage threshold.

When VBUS.UVMODE = 1, an undervoltage fault is issued whenever the DC bus goes below the

under voltage threshold and the controller attempts to enable the drive (software or hardware enable).

General Information

Type

 N/V Parameter

Units

N/A

Range

0 to 1

Default Value

1

Data Type

Integer

See Also

N/A

Start Version

M_01-00-00-000

Variant Supported
MKD EtherCAT Yes
MKD-N Yes
MKD-C No
EtherCAT CoE and CANopen
Index/Subindex Object Start Version

3617h/0

M_01-00-00-000

Related Topics

1   Regeneration