VBUS.UVWTHRESH
Description
If VBUS.VALUE value drops below VBUS.UVWTHRESH, then a warning is generated.
General Information
Type |
NV Parameter |
Units |
VDC |
Range |
0 to 900VDC |
Default Value |
10 volts above the default value of the under voltage fault threshold (VBUS.UVFTHRESH). The default value of VBUS.UVFTHRESH is hardware dependent. |
Data Type |
U16 |
See Also |
|
Start Version |
M_01-00-00-000 |
Variant | Supported |
---|---|
MKD EtherCAT | Yes |
MKD-N | Yes |
MKD-C | No |
Index/Subindex | Object Start Version |
---|---|
3495h/0 | M_01-00-00-000 |
Related Topics
1 Regeneration