WS.ARM

Description

This command sets wake and shake to start at the next drive enable. Feedback type is not relevant for this command. If WS.STATE is 0 and the drive is disabled, then WS.STATE will change to 1 after issuing WS.ARM. With this command, wake and shake can be repeated if desired.

General Information

Type

Command

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

See Also

N/A

Start Version

M_01-01-00-101, M_01-02-00-000

Variant Supported
MKD EtherCAT Yes
AKD-N Yes
MKD-N Yes
MKD-C No
EtherCAT CoE and CANopen
Index/Subindex Object Start Version

3494h/6

M_01-00-00-000

*For PROFINET, write a value of 0 into the PNU to execute a command.

Related Topics

Wake and Shake Overview